Other Parts Discussed in Thread: BQ24745
I have a problem running the BQ24745 Bench Test software wich come with the evalution kit for the battery charger bq24745. I installed the EV2300 driver first as per the instructions. The driver installation succeeded. Then I installed the Bench test software bq24745bench_v141. The installation succeeded, but included a step that was suggesting to me to keep a more recent system file already on my disk. I kept my file already on disk during this installation, and went through therest of installation. Finally The system issued a message telling that the software installation was succesfull. I launched the software, but an error message window came before the software runs. The error message is run-time error 13: Type mismatch. Also once the software runs, I see some kind of window superimposition, I see the window shown on the user,s guide but at the bottom right and on top of another window which shows plenty of status. There is some part of each window that cannot be seen , because one window is on top of the other , and also because the top window (at the bottom right) is limited by the mainframe window of the application. I tried to move the windows but they remain static, I also tried to use the topl menu but nothing happen in any of the menus. Could someone help me to get running the software without errors. The operating system is Windows XP.