Hi
1. What is the maximum power that TPS51225C can provide using charge pump?
Depends on external charge pump circuit?
2. Could it be possible to generate 12V output?
BestRegards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For Charge pump circuit, only suggest to use <10mA as my experience.
if you would to get 12V, use ~3.3V as the charge pump input, that may make the Vout around what you want, but maybe not very accuracy.
Yuchang