This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62142: Radiated Spurious Emission test failing

Part Number: TPS62142

Hi,

In one of our applications we are using this step down converter on a daughter card. And we are undergoing a Radiated Spurios Emmission test in the Band  & Range  4G eFDD12 10Mhz TCH 1200Mhz-12750Mhz HORZ - NB-IOT.

The reason why we think affect is from this device is because when we perform the test without this daughter card it passes the test, when we put this daughter card it fails, the other component on the daughter card is a solar charger device which could not be the source of noise.

I am attaching the schematic, gerbers and the RSE test reports .

Need advise what can modifications can we do on board (put bypass caps, L filter etc..) at the moment to pass this test.20181017_Production_B1PVv06.zip4G eFDD12 10Mhz TCH 1200Mhz-12750Mhz HORZ - NB-IOT.pdf4G eFDD12 10Mhz TCH 1200Mhz-12750Mhz VERT - NB-IOT.pdfSchematicV6.pdf