I don't have hardware yet, so I can't try this out, but reading the datasheets I see an apparent incompatibility between the bq77PL900 and the MSP430 in the area of the I2C interface. The bq77PL900 says that it doesn't send ACKs, but the MSP430 appears to require them and reacts when it doesn't see one. Am I reading too much into this, or is it a real problem which requires a workaround? Does anyone have any proven code to share?
Thanks,
Scott