This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2491: Inquiry about Input Bypass Capacitor( 8.1.2.6 Input Bypass)

Part Number: TPS2491


Dear Specialists,

My customer is considering TPS2491 and has an inquiry.

I would be grateful if you could advise.

---

According to the datasheet P.18, Cin is recommended.

But I'd rather not set input bypass capacitor because inrush current appear. 

Is the input bypass capacitor necessary?

If necessary, what is the recommended capacitor value.

In the 8.2.2.7 Choose R5 and Cin, Cin is recommended in the range of 0.001uF to 0.1uF.

This is a design example , is it possible to think in all cases.

--- 

I appreciate your great help in advance.

Best regards,

Shinichi