This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2491: Question about formula(4) in application note SNVA683

Part Number: TPS2491

Dear Specialists,

My customer is considering TPS2491 and has a question.

I would appreciate if you could advise.

---

Formula (4) in the application note(SNVA683) is listed below. 

VOUTcl = Vz2+Vd1-VTHQ1

where ❏ VOUTCL = Clamped Output Voltage

❏ VD1 = D1 Forward Voltage @ 1 mA

❏ VZ2 = Z2 Clamp Voltage @ 20 µA

❏ VTHQ1 = Q1 Threshold Voltage

Should VTHQ1 use the threshold voltage of the actual FET value ( usually 1~2V)?

Or should I use the gate output of TPS2491(12 ~ 16V)?

I think it should be used actual VTH of  actual FET, is it correct?

I'd like to confirm just in case.

---

I appreciate your great help in advance.

Best regards,

Shinichi