Hi, Team,
For BANK1 non-use pin configuration, is it ok to input FFh for both MSB and LSB when BUF12840 read EEPROM at the start up? The IC is 10 bit, but the customer set all 1 including the upper 6bit.
Configuration
BKSEL pin:0V fix
②Input Data(EEPROM data):
EEPROM address 00h~17h(for BANK0)
:MSB data 00h~03h
:LSB data 00h~FFh
EEPROM address 18h~2Fh(for BANK1)
:MSB data FFh
:LSB data FFh
Best Regards,
Satoshi Yone