Other Parts Discussed in Thread: LM2662, , LM2622
Hello,
I try to boost form an input of 1.5-2.5V (EDLC) to 10V in a two step prozess. First step is to stup-up to 5V with TPS61022 and then doubling voltage with LM2662. The overall current at 10V will be approx. 100mA.
This is the circuit:
I also tried to place D1 between Pin 1 and Pin 8 of LM2662 or not to connect Pin 1 of LM2662. The result is always the same: TPS61022 get defective within 1-5seconds and then has a short. During testing I did not put any load to the system. So current should be 0.
However, if onyl one part of the step-up system is in place, both parts are working as expected. (So if I just build TPS61022 I get 4.99V at its output; or If I just build LM2662 and feed 5V to it, I get 10V at it's output)
Could you please let me know, what's wrong with the combination?
Thank you