This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Step Down Converter solution for Industrial application

Other Parts Discussed in Thread: TPS54560, LM5145, TPS40200, LM5176, LM5085

Hello team,

We have a device that works at 24Vdc and 3A, this is powered by an 18/36 Vac or 24 Vdc source, so we would need a step-down with a 100% duty and I think also a P-channel mosfet is needed.
Because of the voltage drops on the cables it can sometimes happen that the 24 Vdc become 22V, in this case the dc / dc passes everything (minus the DV on the mosfet) or it creates some problem?
This is because I have to control a valve that accepts 22Vdc as the minimum voltage.

Could you please share your thoughts or any suggestions?

Thank you and best regards,

Adrian