Hi,
We currently use the Texas BQ24610 chip to charge a 6.5Ah li-ion battery (robotics application).
In the new version of the robot, 2 packs of 6.5Ah Li-ion battery can be connected in a parallel
- In standard: One 6.5Ah battery (as currently)
- Option: 2 batteries of 6.5Ah in parallel (same specifications, same states, same manufacturing batch).
Allowing, as an option, to double the battery capacity.
Info:
- We cannot use a pack of 13Ah for the option because pack 6.5Ah is certified (FCC, CE, ...) and we must have to use 2 packs in parallel
- The space on the PCB does not allow to use two BQ24610
- Each 6.5Ah battery pack has its own BMS (4-wires output: battery and Smbus)
Do we need a battery balancing circuit for parallel connexion?
I think so because along time, even very identical at the beginning, battries age differently.
Must we balance only during charge and / or during discharge ?
Schematics to propose me?
Regards,
Bernard FROMENT
Electronics Engineer