This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLE4275-Q1: Question about DELAY and RESET port when those are not used

Part Number: TLE4275-Q1


Hi Team,

When user doesn't use Delay and Reset function, could how RESET and DELAY port should be terminated?

Is it OK with below?

- RESET : open

- DELAY  : Short to GND 

Best regards,


  • Hi Fujihara-san,

    When RESET function is not in use, I would recommend having the following connections:

    - RESET : Short to Ground. This is an open-drain output when not in use, it's better to ground it.

    - DELAY : Open. This pin will have smaller current trying to charge it to a threshold, when not in use, better to leave it open to reduce the charging current.

    Regards,

    Jason Song