This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR34215-Q1: Using Electrode Cap as COUT

Part Number: LMR34215-Q1

Hi Team,

My customer would like to use LMR34215-Q1 in below condition.

- Vin range : 9V to 32V, 24Vtyp

- Iout = 0.9A

- Fsw = 400kHz

- Using Electrode Cap (120uF, ESR=25mohm) as Cout

Because this device has built-in compensation, I concern about frequency response with above Electrode Cap.

Q.1) Is there any concern in term of Frequency response with the combination of above Electrode Cap?

Q.2) Can I use LMR36015EVM for Frequency response measurement to evaluate LMR34215-Q1?

Best regards,