Hi
can ISO5852S support 500kHz operation?
thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Max,
Yes, it is possible depending on your operating conditions. Please refer to ISO5852S datasheet Section 10.2.2.9. You may use the equations here to calculate the power dissipation of the driver such that it remains within the safe operating limits of the driver. You will need to know your drive parameters including voltage rails, power switch gate charge, and external gate resistor.
Regards,
Audrey