Hi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Hello Yokoa,
The min peak current is set at 1.23A and this needs to be accounted for when accounting for the max power output capability of the converter. This is worse case at Vin min.
Hope this helps?
Hi David-san
Thank you for the information.
Are there the limitation about minimum load current necessary to use this device?
Hello Yakota-san,
Yes, there is a minimum load requirement for this device, it is set to 0.5% of full load. If this is min load level is violated (Iload <0.5% of Full load) you will experience peak charging on the output voltage. Using a Zener clamp may be necessary to ensure adequate load is provided should Vout increase?
Hope this helps?