This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24092: Temperature fault

Part Number: BQ24092
Other Parts Discussed in Thread: BQ24040, BQ24086, BQ24081

Hi,

We are using BQ24092 in one of the consumer product to charge a single cell Li-ion battery. In the product we have connected a bi-color LED to the nPG and nCHG pins, a temperature sensor on the TS pin (10K NTC). When the battery is charging both the LED's are ON and working normally, but when there is battery temperature fault the LED indication for charge complete/charging are same. With this how we can differentiate whether the charging is completed or there is a battery temperature fault through LED's. 

We need both the LED's to be OFF when there is battery temperature fault (Similar to OV/UV fault condition). 

Thanks,

Sreekanth