Hello,
I am currently using Fusion digital designer to set two ucd9248 devices for 8 power rails.
I uses design to set my current voltages setting
put even I got good monitoring values (except rail#1 53h which has been destroyed):
The outputs measured with a voltmeter are completely different:
ucd 52d rail#1 is 2.2V instead of 0.95V
ucd 52d rail#4 is 3.2V instead of 2V
etc..
could you tell me what could be wrong in the process of setting ucd9248 device through Fusion Software ?
Thank you