Hello,
We are using TPS63070 Buck Boost regulator in our application. PFA Buck Boost section of our application.
We are giving 9-15 V as Input and we want 5V as output.
The enable pin is dynamically controlled to ON/OFF the regulator.
The Buck Boost does not start even after giving high to the ENABLE pin of the regulator.
When the ENABLE pin is given high the TPS63070 reaches a maximum of 0.59 V and does not give the desired 5V.
Please advice the reason why it could be and the solution for it.
Thanks,
Ameya