Hello E2E,
I looking for Low-side gate driver that it has 2-channels output and adjustable dead-time feature.
Does TI have any matched device?
Regards,
ACGUY
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI ACGUY,
Thanks for reaching out on e2e,
Typically adjustable dual channel drivers come in half-bridge configurations rather than dual low-side drivers. You can use LMG1210 which is a half bridge driver as two low-side drivers by grounding the HS pin. LMG1210 has an adjustable dead-time feature 0.5ns to 20ns. What max/min dead-time do you require? You can also use a single or dual channel driver with a LPF on the inputs to form a fixed dead-time. LMG1210 can drive MOSFETs or GaN FETs with 5V VDD drive. What gate drive voltage do you require?
Thanks,
HI ACGUY,
Do you require isolation? what application is this for?
Other half bridge drivers that can be converted to low-side drivers with dead-time are UCC21520 (and UCC21222) as well as LM5106.
Please let me know if you have any other questions.
Thanks,