Other Parts Discussed in Thread: TLV61048
Hi there,
I have a system supplied by a litium battery and I need to generate 12V and 3,8V. For the 12V generation I've choosen the LMR62421.
To minimize the number of different references I'm thinking of using the same ic to generate 3,8V, but the battery goes from 2.7V to 4.2V. I've seen in the datasheet that the LMR62421 can be used as SEPIC converter, but the example uses the WSON package, Can I use the SOT-23 package as SEPIC converter too? I wpuld like to confirm that because we are soldering ir ourselfs and the SOT-23 is easier to solder.
it would be a problem if I design the generation of 3.8V with the LMR62421 as boost controller? I mean, is there a problem if I have a 2,7 to 4,2V input and I use the LMR62421 as boost controller to generate 3,8V output? How would it work with a Vin > Vout?
Thanks in advance,
Regards,
Ainara