Other Parts Discussed in Thread: BQ4050
Hi ,
After editing the data memory in such way that all the "ENABLE PROTECTIONS" are disabled, in addition , non of the hardware protection flags are on, the XDSCH and XCHG flags are set , which means that voltage do not transfered from the pack pin to the batteries and the fets are closed. It contradicts the fact that i disabled the protections. (the flags which are set are CUV,UTD and UTC, the temperature at the auto refresh main panel shows -273 degC and the voltage shows 0 mV) . how can i solve it ?
Best Regards,
Arkadi