This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: On 1S3P pack, bq loses communication on CUV condition.

Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: BQSTUDIO,

Working with a pack of 3 parallel-connected cells and attempting to discharge the pack to the minimum cell specification (2V). I've had to adjust CUV upward from 2V to ensure the bq remains above its operating voltage (2.2V). Every time the pack crosses CUV, the chip goes unresponsive to bqStudio despite having adequate voltage to run the chip (e.g. 2.4V). I've adjusted all "Power" thresholds far below 2V to ensure they don't function and CUVC is disabled.

How do I ensure I can reach CUV without the chip shutting off?