This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS / LMR14030-Q1: Can the LMR14030 replace the MP2229?

Part Number: LMR14030-Q1


Tool/software: Code Composer Studio

1. MP2229 is a chip with adjustable output and soft start time of ns. Can I use LMR14030-Q1 to replace it with PIN 2 PIN?

2. I see the soft start time of the LMR14030-Q1 in the manual is 5ms. I understand it?

Thank you!

mp2229.pdf