Hello, I’m using BQ24079 operated from USB port (5v). In the datasheets states that " OUT provides a regulated output when the input is below the OVP threshold and above the regulation voltage (5,5V for BQ24079). So the question is...Can I Have the regulated output if the power source for charging the battery and running the system is a USB port? I think not, so which output will I have? Should i change it for a BQ24073 which has a regulation voltage 4.4V?
Ps: Sorry for my bad English is not my first language.
Thanks!