Input /Output voltage is 8~32V(12V/24V Typ, 1A Current), The battery as a backup power when no Input, The battery Spec: 7Cells, Voltage 28V Max (no the 26V type) , When used BQ24620 the battery cells can't charged fully for only 26V Max, that will cause bad impact.
How we can solved such issue? Give a booster after battery or booster after Input or any solution ,Please help check the Issue,Thank you!