This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Asking for the recommendation on the charger solution and design

Other Parts Discussed in Thread: BQ25606, TUSB320

Hi Team,

Customer is looking similar version to BQ25606 but with I2C. 

Customer is thinking to use TUSB320(as UFP) to detect type C host current capabilities, and use the GPIO output of TUSB to change I_CHG of the BQ25606. Do you think it is workable, because the BQ25606 will detect USB SDP (USB500) from D+/D-,limit the input to 500mA, and ignore the I_CHG.
Is it correct?

Would you please recommend the proper solution for this?
Could I2C be used to override the detection and the input current limit? Or it cannot?

 

 

 

 

 

BR,

SHH