Hi there, I wanted to confirm with a specialist that my schematic design is optimal for what I want to do. I used a lot of the information provided from both the datasheet and the TPS61175EVM-326 . My device takes an input voltage of 15V and outputs at 24V. which from the equation for max output current gives me 1.5A. Attached below are the values I have chosen for the passive components to the schematic. Please let me know if you have recommendations for changes or anything. Thanks!