Hi all,
I’m having issues with the bq76200 in my hardware. My minimal setup is:
Pins DSG and CHG are left open, not driving any MOSFET, to make debug easier.
PACK+ is 25VDC, and voltage reaches pin 11 fine
BATT+ is 36VDC, and voltage reaches pin 2 fine.
RC filters to BAT and PACK pins are as specified by datasheet, using X7R 50V ceramic caps.
CP_EN is 3V, and CP cap has a voltage of 10.3VDC when CHG_EN and DSG_EN are 0.
CP Cap is 2.2uF 35V ceramic, very close to pins 1 and 2.
With CHG_EN and DCHG_EN both in 0, CHG pin copies BAT, and DCHG pin copies PACK.
My first concern up to this point is, why would I have a CP voltage of only 10.3V (almost in the UV limit of 9V), and not something more similar to 12 or 14VDC?
For the test, PMON_EN and PCHG_EN are driven low.
When I drive high CHG_EN (with 3V), leaving DCHG_EN low, CHG pin goes almost to BAT + Cap CP voltage, and voltage across CP cap stays in 10.3V. I guess this is fine, as it’s more than enough to turn on my unconnected MOSFETs.
When I drive high DCHG_EN (with 3V, leaving CHG_EN low), voltage across CP cap drops to 9.5V, and the pin DSG goes to only 28VDC, 3V over PACK pin.
When I drive both pins CHG_EN and DCHG_EN high, CHG pin stays in BAT voltage and DCHG pin goes to PACK voltage + 1.5V, and CP cap voltage is at 9.5V
For my understanding of the datasheet, I’m having under-voltage detection reading over the CP cap voltage in the bq76200 when driving high DSG_EN pin, but i’m not sure. Even if this is happening, I don’t understand why, as the CP cap value is fine (pins are not driving anything), and it’s well positioned in the layout.
I changed the bq76200 just in case it was faulty, but the problem persists. I still read the 2.2uF across the cap, so the cap is not damaged.
Please, any help will be much appreciated.
Thanks very much,
Sebastian