Other Parts Discussed in Thread: UC2842, UCC28C42, UC2843
Hi, I am Tri from Vietnam.
I am doing the DC-DC 230VAC to 12VDC application. And UC3843 is used in this case. But I get stuck to some problems. Please help me to solve it!
Question 1: I'd like to ask about two diodes Zener between VCC & OUTPUT and OUTPUT & GND pins, I don't see any recommendations or equations to calculate this one. Could you please tell me how to determine it? ( I chose diode Zener 18V-1W between VCC - OUTPUT, 12V-1W between OUTPUT - GND by myself, is it right?)
Question 2: I chose Css = 10 nF and Rss = 10k ohm in Solf Start function, is it ok?
Question 3: Because I see Design Example Schematic on page 22 use UC2842. So if I use UC3843, do I need to change any components or parameters?
Note: Fsw is selected to be 110KHz same as example schematic.