This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25927: Conditions described in UL File No.

Part Number: TPS25927

UL File No.E339631 wrote.
Volts 4.5 to -18 VDC
Cont.Current 4.15 to -4.5
Prot.Current 5 to -5.7
Temp Range 30°C to -70°C

I assumed the following
Volts 4.5 to 18 VDC
Cont.Current 0 to 5
Prot.Current 0 to 5
Temp Range -30°C to 70°C

Are the voltage, current, and temperature listed in the UL File No. correct?
If so, please tell me why. If there is a mistake, please tell me the correct value.