Hello,
I have the problem to solve that I need a test board for USB C PD.
There are finished test applications availabe, but no one can really solve all problems.
I need a test board (or a combination of boards) where i can test any case that can happen by using the USB C PD up to 20V & 5A.
Cases like USB C connected to an USB B Port, connections without using an EMCA cable, or what will happen if the communication between Host, Client and EMCA is disturbed.
Do you have any idea or experience in this case?
greetings
M. Schian