Hi Team,
In the data sheet it shows for current capability for the TPS65185:
TPS651851 |
3V Max (mA) |
3V6 Max (mA) |
|
VGH CP1 |
15 |
Max |
|
VGL CP2 |
15 |
Max |
|
VPOS LDO1 |
150 |
200 |
Max |
VNEG LDO2 |
120 |
200 |
Max |
VCOM |
15 |
Typical |
If my customer performs some screen blanking and writes a complex 1-bit dithered image to their display they get #s such as:
max(mA) |
min(mA) |
RMS(mA) |
Waveform No. |
|
VGH |
30.8 |
NA |
3.86 |
35 |
VGL |
12 |
- 34.4 |
4.6 |
36 |
VPOS |
30 |
- 8 |
6.6 |
37 |
VNEG |
16 |
- 150 |
39.9 |
38 |
VCOM |
58.8 |
-17.2 |
4.12 |
39 |
These peaks exceed the data sheet, but the RMS # is in line with the data sheet. Can you help me understand if they are in violation?
Thanks,
Mitchell