This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Performance of the Push-Pull LLC Resonant and PWM ZVS Full Bridge Topologies

Other Parts Discussed in Thread: UCC28083

Hi TI Team

I have a case/project design a power converter.

The input voltage is 48V fixed, the output is adjustable and the maximum voltage is 60V, the maximum current is 20A, and the maximum power is 200W.

I'm thinking could I design a converter Push-Pull LLC (primary) Resonant and PWM ZVS Full-Bridge (secondary)Topologies.

 

This thesis focuses on the study and implementation of an
interleaved series resonant converter (SRC) with a secondary-side
resonant tank. The conventional half-bridge SRC is not suitable for low input voltage
and high output voltage applications.

I sought some literature.

https://scialert.net/fulltext/?doi=jas.2011.2744.2753

http://asokatechnologies.in/tag/push-pull-converter/

Do you have any control IC could achieve this application??

Thanks