Hi,
Switching frequency depends on VDD on customer's circuit.
It is 86kHz at VDD=12V, it is 84kHz at VDD=30V.
Is this variation valid?
The RC pin is connected with VDD via a resistor on the schematic.
RT and CT connected with RC pin are 680kΩ and 220pF
Best Regards,
Kuramochi