This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61194-Q1: PWM pin of TPS61194-Q1

Part Number: TPS61194-Q1

Hi , 

I am connecting TPS61194-Q1 PWM pin to a MCU , in that at when PWM pin is pulled ground ( continuous zero ) the screen turn blank , Can I or the PWM signal with Vref ~1.2V & then give to PWM pin so when the PWM from the MCU is pulled zero , VREF appears at PWM pin . Is this acceptable , because as per internal  block diagram of IC it needs PWM to control brightness . 

Please guide me. I basically need a min brightness , the screen should not turn blank. 

Gaurav