This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54361: usage of series resistor to bootstrap cap

Expert 4495 points
Part Number: TPS54361


Hi,

Do you expect issues when using a 20 Ohm series resistor to a 100nF bootstrap cap as shown in below picture? Max Fsw is 500kHz. Max output current is 2A, 5V. Input voltage range from 18V to 35V.

Thanks & BR,

KF