Need topology advice for designing 1100 W DC-DC power supply.
- Input: 300 Vdc
- output: 90 Vdc
- Output power: 1100 watt
- Isolation: 2 kVac
Looking for help to get idea for topology and device selection.
Thanks,
Parth
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Need topology advice for designing 1100 W DC-DC power supply.
Looking for help to get idea for topology and device selection.
Thanks,
Parth
Parth
At this power level and voltage we recommend using a phase shift full bridge converter with UCC28951. This device is designed to support isolated DC/DC with similar voltages for both input and output at this power level.
The isolation rating is determined by the magnetic components and gate driver used.
Best Regards,
Eric