This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Golden Image with loads below C/20

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQ34110

We are using a bq34z100-G1 part to fuel gauge three battery packs where the load is a constant current of less than C/20. The application typically takes 3-5 hours with a maximum of 16 hours of operating time before recharging. I picked a battery chemistry of 0100 for my LiCoO2/graphitized, carbon, 18650 cell from Panasonic (or Samsung). Is this image good enough to serve for our application? Say for a few adjustments, e.g. Design Capacity of 4.8 Ah. I expect 3-5% error on Remaining Capacity as opposed to 1% error -- this should make little difference to the user. Besides, it is unclear to me what learning cycle currents would apply from such a small current load that is below C/20.

  • Hi Graham,

    At a load of C/20 you will not update resistance values. You need a rate > C/10 for Ra updates. For such low loads, you may want to look up the bq34110. It's a simpler gauge and is slightly less accurate but can work with low currents as it's based on a different algorithm.

  • I can understand that the Learning Cycle wouldn't be very successful with a C/20 load, but I don't understand why an Impedance Track fuel gauge wouldn't perform well with a lightly loaded battery.  Referring to Figure 3 in SLUA450 (for example), it seems to me that as battery capacity is consumed, there would be plenty of dV to be measured and thus Ra calculations could be made.  Am I missing something fundamental?  Thanks... 

    Chris

  • Hi Chris,

    We keep the battery in specific modes, chg, dsg and relax based on current thresholds. At low rates of dsg, you are typically depending on OCV to update capacity rather than a combination of coulomb counting and DOD updates. This happens when you have C/20 or so rates of dsg. We will update resistance only when the rate of dsg exceeds C/10. That's why we advise you to use a C/10 rate at a minimum.

  • Hi again.  I have a lingering worry that I didn't state my question clearly enough, because it doesn't seem right that an impedance-track fuel gauge would work well only if battery lifetime between charges is less than 10 hours. 

    To be specific, for a 2.4-Ah battery, if we use a >240-mA dsg rate during the Learning Cycle, would the bq34z100-g1 perform well in a system where the actual load range is 50-120 mA? 

    Thank you.  I appreciate TI's excellent customer service in this forum!

  • Hi Chris,

    If you have programmed and learned your battery correctly, yes, with a 120mA dsg, you will learn resistance and qmax if you exceed the chg and dsg thresholds. If your load is going to be 50mA at a minimum I suggest setting your chg and dsg current thresholds to 45mA.

    Thank you for your kind words. We wish you success in your application.