This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53355: Power management forum

Part Number: TPS53355

Dear,

     Now we design a new board ,there is a power cuircit with TPS53355,  Vout= 0.6*(1 +R1/R2).

     There is a question:

     In the whole cuircit ,most needed devices were solded,but only  R1 wasn't be solded,I want to know what will happen?How wii the  Vout  be, will the Vout be very high and burnout the load?

     Thanks!

yours

Jo

     

  • Jo,

    Because IC uvp enabled 1.5ms after soft-start done, so IC detect Vout is lower than target after FB connected to GND with R2, PWM will be generated continuously to charge Vout during uvp disabled, then Vout will go higher level. And after soft-start UVP will be triggered...

    So If R1 is not stuff, Vout will go higher, may cause the load damage if over voltage stress of the load,

    Yuchang