Hi team,
My customer would like to use the TPS54202 for the following condition. Could you let me know the recommended inductance value and how to calculate?
Vin : 10V to 20V
Vout : 3.3V
Iout : 20mA
According to the equation 8 in the d/s, the inductance would be 842uH(min) at the customer's condition. On the other hand, Webench recommends 220uH (189.1uH to 378.1uH). I don't think that this design requires such a large inductance. I believe that the equation 8 is for CCM.
Anyway, could you let me know the recommended inductance and its equation?
Regards,
Yamaguchi