Hello All,
I am new in this designing. I want to design 350W buck converter with multiple output(+12V, +5V, +3.3V & -12 V). My problem in buck circuit is that to convert (90V to 180V dc, Nominal 120V DC) into DC (+12V, +5V, +3.3V & -12 V). I don't know which buck method is better and efficient and which controller should i select for that converter. I will used this converter in running my computer through 120V DC BUS. Please help me to start and design.
Thankyou in advance.
Regards,
Shwetank