This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28951: Inner current loop

Part Number: UCC28951

Dear All,

I have selected UCC28951 for my converter. 

For overcurrent protection,  the controller IC is having a CS pin. If the voltage exceeds the 1.8 V the short circuit protection will come into the picture. 

Actually I need the inductor current control as well as output voltage control also. I can able to see only one comparator is available in the controller for voltage mode control. 

Please let me know the possibilities of using both current and voltage control.

Thanks and Regards

Prakash.S