Other Parts Discussed in Thread: UCC28180, UCC28180EVM-573
Dear Friend;
Vout:50W,Vin:230VAc. UCC28056 THD<6%,Whether it can be implemented !
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Friend;
Vout:50W,Vin:230VAc. UCC28056 THD<6%,Whether it can be implemented !
Thank you
Hello Tony,
The UCC28056 transition mode PFC pre-regulator has shown THD performance of less than 18% from 50% to 100 load. Please refer to figure 6 in the EVM users guide for THD performance.

For sub 6% at full load you should consider using the UCC28180 which can achieve less than 22% THD at 20% load at 230V RMS and less than 8% at full load.
Figure 5 in the UCC28180EVM-573 shows typical THD curves for this topology.

Design information can be found in the UCC28180 data sheet. http://www.ti.com/lit/ds/symlink/ucc28180.pdf
There is also a Webench design tool available to aid in y our design. http://www.ti.com/product/UCC28180/toolssoftware
Regards,
Mike