This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650EVM-639: BQ24650EVM-639 R1 R2 functions

Part Number: BQ24650EVM-639

hi  Team:

in the  BQ24650EVM-639 ,What are the functions of R1,R2?How to select parameters?Is it related to the input power or the output power?

  • Hi David,

    R1 and R2 in parallel are approx. 2ohm and, along with C4, are used to damp voltage ringing when the input source hot plugged.  If not damped, a high voltage power source could ring up over the charger's abs max at plug in and damage the charger and/or the input FETs.

    Regards,

    Jeff