This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS56221: TPS56221 PGD pin quesition

Part Number: TPS56221

Hi team,

Our customer pull up PGD pin of TPS56221 to input voltage wrongly(input voltage is 14.5V, pull up resistor is 3.3kohm), we know that the maximum voltage of this pin is 7V, but as customer can`t modify the circuit currently, so they wonder if this connection will damage the device?

As I know most of our IC pin has ESD protection diode, max current is 5mA generally, so I ask customer change the pull up resistor to 100kohm, but I am not sure if this solution if safety for TPS56221?

Or do you any other solution?

Thanks very much.

Regards, Sunny