Hi,
We are trying to use the UCC25600 to LLC power supply, now under debugging.
But when start up, device found inrush current as overcurrent, then goes shout-down rapidlly during 2-3ms.
We are looking also SS pin (as start-up enable), but seems to be kept low level (around 0.6 to 1.0V) even if we try to start.
Well one question is, this is right operation using to LLC ?
We guess resonant capacitor is one of factor to occur such as issues. However we will not change this capacitor7s value and types.
Therefore we try to control DC current level using RC network between OC pin and current sense circuit, we can avoid this issue.
So Do you think it is better resolution?
Best regards, Keiichi