This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A24: about R1&R2 value

Part Number: TPS7A24


Hi,

We plan to create a 9V output from a 12V input using TPS7A24.

Please tell us the recommended resistance values for R1 and R2.


The minimum value of the input voltage is 10.8V,

the load current is typically 50mA and the maximum is about 110mA.

Best regards,

  • Hello,

    The final datasheet is not completed yet for this component, but when it does come out you will want to confirm the necessary headroom will meet your needs with 110mA maximum load. 

    Choosing E96 1% resistors, 84.5K for the high side resistor and 13.7K for the low side resistor will produce quality results.

    Thanks,

    - Stephen