Other Parts Discussed in Thread: TPS63802
Hi
In TPS63020 datasheet, output current is mentioned as 2A and the conditions are Vin>2.5V and Vout=3.3V. The max switch current mentioned as 4A.
My question is by which calculation we are getting 2A current @ 3.3V out? I need to find the max current at Vin=3.3V, Vout=5v so how can i calculate this?
And in one of the generic document (SLVA372C), for getting maximum switching current (Isw(max)) we need to get the Ilim(min) {refer page no.2 }. From where we can get this Ilim(min) in this TPS63020 datasheet?