This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: Problem with Gauging Parameter Calculator

Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQSTUDIO

Hello, 

i have uploaded my logging files for CEDV into the  GPC but everytime i do so, i receive an error (specific reason was not identified). I have prepared my files as it is requiered in the description. 

One more thing: The files are sample files (6 equal files) but that should not be problem if i am not wrong. 

Thank you !

  • Hi Alexandros,

    If you are using 6 equal files, did you name the files according to the instructions (they should have the 6 names specified)? If you need help creating the zip file correctly, there is a GPCPackager Tool in BQStudio when using the BQ78350-R1. This app note has the instructions specific for this device: http://www.ti.com/lit/an/slua924/slua924.pdf

    If you still have trouble after trying these steps, you can send me your zip file and I can try to see what might be wrong.

    Best regards,

    Matt