This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61030: TPS61030 - short between SW and GND

Part Number: TPS61030

Hello,

my TPS61030  board generally working fine. (3.2V battery to 5V)

After some time of testing the board stops working, short between SW and GND.

I can not say exactly when it happens. My guess is that it happens i plug in the battery connector.

Battery is connected by 10cm of wires to the board.

Can you please check my layout?