Other Parts Discussed in Thread: PGA460
Good day,
I am using tlv61046a to drive/power up PGA460 that is being run in transformer driven bistatic mode at 58 and 200 kHz frequencies.
With reference to the application note (attached), is it recommended to incorporate solution 2 as mentioned in the app note i.e. using P-FET and zener diode to connect the load (pga460) after Vout is stable?
In the present case, Vout is set to 8.4V.
Another way might be to skip the startup solutions mentioned in the app note and configure/access the PGA460 sometime (100 ms) after the tlv61046a is turned on.
Thanks